NX5P3290: The output has a voltage drop of about 0.1V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NX5P3290: The output has a voltage drop of about 0.1V

Jump to solution
584 Views
Peiwu
Contributor I

Hi All:

I used NX5P3290UKZ in my design, but when the VIN is 5V, the VBUS output is only about 4.9V (without load). I didn't see any description of voltage drop in the datasheet. Is this correct? What is the cause? 

Theoretically, the output voltage should be equal to the input voltage.

My schematic is as follows:

Peiwu_0-1660228939772.png

 

0 Kudos
Reply
1 Solution
569 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

NX5P3290 has a function to make VBUS=Vin-70mV, so yes It is normal to have a small drop in output with no load.

Regards.

View solution in original post

0 Kudos
Reply
1 Reply
570 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

NX5P3290 has a function to make VBUS=Vin-70mV, so yes It is normal to have a small drop in output with no load.

Regards.

0 Kudos
Reply