NX5P3290: The output has a voltage drop of about 0.1V

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NX5P3290: The output has a voltage drop of about 0.1V

跳至解决方案
580 次查看
Peiwu
Contributor I

Hi All:

I used NX5P3290UKZ in my design, but when the VIN is 5V, the VBUS output is only about 4.9V (without load). I didn't see any description of voltage drop in the datasheet. Is this correct? What is the cause? 

Theoretically, the output voltage should be equal to the input voltage.

My schematic is as follows:

Peiwu_0-1660228939772.png

 

0 项奖励
回复
1 解答
565 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

NX5P3290 has a function to make VBUS=Vin-70mV, so yes It is normal to have a small drop in output with no load.

Regards.

在原帖中查看解决方案

0 项奖励
回复
1 回复
566 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

NX5P3290 has a function to make VBUS=Vin-70mV, so yes It is normal to have a small drop in output with no load.

Regards.

0 项奖励
回复