NX5P3290: The output has a voltage drop of about 0.1V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NX5P3290: The output has a voltage drop of about 0.1V

ソリューションへジャンプ
581件の閲覧回数
Peiwu
Contributor I

Hi All:

I used NX5P3290UKZ in my design, but when the VIN is 5V, the VBUS output is only about 4.9V (without load). I didn't see any description of voltage drop in the datasheet. Is this correct? What is the cause? 

Theoretically, the output voltage should be equal to the input voltage.

My schematic is as follows:

Peiwu_0-1660228939772.png

 

0 件の賞賛
返信
1 解決策
566件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

NX5P3290 has a function to make VBUS=Vin-70mV, so yes It is normal to have a small drop in output with no load.

Regards.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
567件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

NX5P3290 has a function to make VBUS=Vin-70mV, so yes It is normal to have a small drop in output with no load.

Regards.

0 件の賞賛
返信