NHS3152: flashing the device via NFC while NFC powered

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NHS3152: flashing the device via NFC while NFC powered

Jump to solution
1,947 Views
CyrilBZH
Contributor I

Hello,

I'm using the NHS3152 in a project for which the NHS3152 is NFC powered.

So far I'm using the NHS3152 ADK board. The program flashed using the LPC link2 works fine on the NFC-powered chip.

However, I won't have room on the final product PCB to connect the programming pins.

The device can be flashed via NFC, but is it possible  to NFC flash the chip while NFC powered?

I couldn't find that info in the documents.

Best regards

Cyril

0 Kudos
Reply
1 Solution
1,877 Views
patrickgeens
NXP Apps Support
NXP Apps Support

Hi CyrilBZH,

 

Sorry for the late reply, I probably forgot to click the POST button

 

Yes, in that case flashing via NFC is possible.

Note that the programming speed is slow compared to SWD programming, not really useful for mass production.

 

Kind regards,

Patrick

View solution in original post

0 Kudos
Reply
5 Replies
1,930 Views
CyrilBZH
Contributor I

Thanks Patrick,

then, would it be possible to NFC flash if I manage to power the chip during flashing using a 3V3 DC power source ?

best regards

Cyril

 

0 Kudos
Reply
1,878 Views
patrickgeens
NXP Apps Support
NXP Apps Support

Hi CyrilBZH,

 

Sorry for the late reply, I probably forgot to click the POST button

 

Yes, in that case flashing via NFC is possible.

Note that the programming speed is slow compared to SWD programming, not really useful for mass production.

 

Kind regards,

Patrick

0 Kudos
Reply
1,872 Views
CyrilBZH
Contributor I
Hello Patrick,

thanks a lot.
best regards
Cyril
0 Kudos
Reply
1,933 Views
patrickgeens
NXP Apps Support
NXP Apps Support

Hello CyrilBZH,

 

Flashing on NFC power only is not possible: to replace the reset vector from default NFCloader firmware to the new firmware, an erase cycle is needed (happens at the end of the NFCloader operation). This causes the internal voltage to drop too low, causing a reset of the system. Typically the reset vector is then already erased or damaged, so NFCloader firmware will not start again. You can recover only by SWD programming.

 

Kind regards,

Patrick

1,929 Views
CyrilBZH
Contributor I

Thanks Patrick,

then, would it be possible to NFC flash the chip if I manage to power the chip using, say,  a 3V3 DC source during flashing?

Best regards

Cyril

0 Kudos
Reply