NFC reader library porting to BGM13S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC reader library porting to BGM13S

422 Views
yamuna_gadari
Contributor I

Hi 

I'm using CLRC663 plus and BGM13S, and i wanted to port the reader library to BGM13S. I followed porting guide  NFCReaderLibrary_IMXRT1050_CLEV6630B_Porting_Guide . And I followed all the steps given and made changes according to BGM13S. I'm able to read the VERSION_REG from CLRC663, but when i debug the code line by line, in discloop_run() the control is going to default handler and also it is returning DISC_LOOP_FAILURE.

 

Thanks & regards

Yamuna

0 Kudos
1 Reply

416 Views
nxf58474
NXP Employee
NXP Employee

Hi Yamuna,

 

Sorry for the inconvenience this might cause you, but we do not provide support on migrations of the NXP NFC Reader library, and we cannot help you with your specific MCU as we do not have a way to test the device as it is not from our company.

 

Maybe these other guides for the migration process would be helpful:.

  • Porting NFC Reader Library to Kinetis K64 | Document | Video
  • Porting NFC Reader Library to LPC11u37h | Document I, II, III, IV

 

Best Regards,

Ricardo

0 Kudos