NFC cockpit Installation failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC cockpit Installation failure

866 Views
ykt
Contributor I

Hi all

When I try to install NFC Cockpit (ver05.03.00) on a PC (Windows 10 64-bit), the installation fails like the attached file. (Even if OM27426CDK is connected, it cannot be recognized from the NFC cockpit.)
I tried several times, but it fails. The same result was obtained when I tried it on another PC.
(Device Manager recognizes OM27426CDK normally.)

Please advice.

Tags (1)
0 Kudos
2 Replies

855 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

We have not OM27426CDK kit. Would you please double check again?

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos

842 Views
ykt
Contributor I

Hello TecSupport

Thank you for reply.

I’m so sorry that I mistook model number.

NG:OM27426CDK    ---> OK:OM27462CDKP

I also tried installing it on a LENOVO PC (windows 10 64bit) and an NEC PC (windows 7 32bit), but it didn't work as well. (The right side of the application becomes "white".
Are there any conditions to install NFC cockpit?

Please  advice

0 Kudos