I have a tag that I'm evaluating for a development project. It incorporates a SL2S2602 ICODE SLIX2 IC. I'm using the NXP TagWriter Android App from Play Store to do my evaluation. The tags that I'm evaluating are on a roll. When I lay the roll out and quickly place my Android device over 2 tags, neither is read and NFC reading on the Android device is disabled (i.e. can't read tags). I must either restart the device or disable/re-enable NFC in settings to get the device to start reading tags again, I've seen this behavior on CAT S41 with Android 8.0.0 and Samsung S9 with Android 9.0.0. I did not see this behavior on Kyocera E6810 with Android 7.1.2 or Huawei MHA-L29 with Android 8.0.0. I also tried this with SL2S2002 ICODE SLIX tags (saw same behavior) and 14443 tags (did not see same behavior). Has anybody seen anything similar?