Minimum rise and fall time (Fast mode) of I2C bus signals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Minimum rise and fall time (Fast mode) of I2C bus signals

ソリューションへジャンプ
1,468件の閲覧回数
Danz1
Contributor III

Hi,

For the minimum rise and fall time (20+0.1Cb) requirements, does it applies to signal going into the I2C device? Am I right to say it is not critical if the signal is going out of the I2C device? 

 

Danz1_0-1689910218431.png

 

Rgds

Danz

0 件の賞賛
返信
1 解決策
1,447件の閲覧回数
Danz1
Contributor III

Hi Jozef,

Thanks for your reply.

Rgds

Danz

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,451件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Dan,

yes, this is correct. The minimum values are critical for the SDA and SCL inputs.

With Best Regards,

Jozef

0 件の賞賛
返信
1,448件の閲覧回数
Danz1
Contributor III

Hi Jozef,

Thanks for your reply.

Rgds

Danz

 

 

0 件の賞賛
返信