Maximum frequency for TEA2209T

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum frequency for TEA2209T

198 Views
ovsiyenko
Contributor I

Hello to all,

I am thinking of using the TEA2209T as a rectifier for my project. I have an AC input signal of 85 kHz frequency, would it be possible for this controller to rectify this high frequency signal rather than Hz from mains?

Regards,

Denys  Ovsiyenko

0 Kudos
Reply
1 Reply

181 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

The Maximum operation frequency is ~ 800Hz.

0 Kudos
Reply