Max damage input power to BFU580Q Transistor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Max damage input power to BFU580Q Transistor

610 Views
m35gP91
Contributor I

What is the max damage input power to BFU580Q NPN wideband silicon RF transistor?

0 Kudos
Reply
1 Reply

595 Views
LPP
NXP Employee
NXP Employee

The maximum RF input power may depend on the amplifier design.

Typical limit is determined by the voltage swing at the transistor base. Having in mind VEB=2V max and VBEF=0.6V, RF input power should be less than about 12dBm at 50 Ohm input impedance.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply