Max damage input power to BFU580Q Transistor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Max damage input power to BFU580Q Transistor

669件の閲覧回数
m35gP91
Contributor I

What is the max damage input power to BFU580Q NPN wideband silicon RF transistor?

0 件の賞賛
返信
1 返信

654件の閲覧回数
LPP
NXP Employee
NXP Employee

The maximum RF input power may depend on the amplifier design.

Typical limit is determined by the voltage swing at the transistor base. Having in mind VEB=2V max and VBEF=0.6V, RF input power should be less than about 12dBm at 50 Ohm input impedance.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信