Dear Community,
in the macro, the cell map is intended for 7 cells. I would need it for 12 cells. How do I know or find out which value I have to enter?
best regards,
Patrick
Hello Patrick,
The mentioned macro is a part of the driver internals. The number of cells has to be defined in the configuration structure bcc_drv_config_t.
The example of the driver intialization can be found in the example project BCC_S32K144_Monitoring, which is a part of the driver package. Specifically in the file main.c, function static void initDemo(status_t *error, bcc_status_t *bccError).
If you require any further information, let me know.
Regards,
Jakub
Dear @TomasVaverka,
I got this from the data sheet in the BCC_SDK_SW folder. Embedded SW: MC33771/MC33772 SW Driver | NXP Semiconductors
best regards,
Patrick
Hello Patrick,
I am not sure which code/project this macro is from. Could you please provide me with this information so that I can contact the appropriate SW engineer?
BR, Tomas