Hi,
I have 2 MRF13750 that went up in smoke quickly. I wonder if this is how they should look inside?
Best regards
Hi Erica thanks for reply.
I use this design as in the photo. And one more picture of a unit that crack instantly.
I bought 3 units from a seller on EBay for $160 each. One unit seems to be alive, but only deliver 50W out with 2W drive (should be 200W).
It does not seem to be any of our reference designs so we can not ensure its performance of it, in this case, please ask the designer so he can give you some advice, for my part I recommend you to do the following:
Hope it helps.
Hi Erika,
Thank's for answer. No it is based on the original design. The question is if the inside looks like it should.
Of course not the burnt location.
Lasse // SM6WHY
Hello,
No, they definitely should not look like that, are you using one of our reference designs, if so, which one?