MPC8315e TDM bus for si3015 codec

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8315e TDM bus for si3015 codec

Jump to solution
937 Views
uolli
Contributor III

does any one who tried MPC8315e tdm bus with si3015 codec? i am trying connecting the MPC8315e TDM bus with Slicon Labs si3015, but can't get the timeslot working properly :smileysad:. for example, when i used the mpc8315e tdm bus driver setting with no bit delay for FSYNC as following shows

-------------------------------------------------------------------------------------------------------------

        out_be32(&priv->tdm_regs->rir,
                 RIR_RFWM(0) | RIR_RFEN | RIR_RWEN | RIR_RDMA | RIR_RSL |
                 RIR_RSO | RIR_RCOE | RIR_RRDO | RIR_RFSD(0x0));
        out_be32(&priv->tdm_regs->tir,
                 TIR_TFWM(0) | TIR_TFEN | TIR_TWEN | TIR_TDMA | TIR_TSL |
                 TIR_TSO | TIR_TRDO | TIR_TFSD(0x0));

-------------------------------------------------------------------------------------------------------------

also, following the si3015's datasheet, there is no need FSYNC delay for channel 0 in RXS/TXS equal 0. but i can't get any voice from si3015, just noise. when i changed mpc8315 tdm bus with one FSYNC dealy, i can got very cheap voice (can't useable) :smileysad:

this is very strange, i have spent two days on this, but not any progress. so, anyone who has some experience on mpc8315e tdm bus can give me some suggestion will be very appreciate!

 

Best regards,

Li

0 Kudos
1 Solution
443 Views
uolli
Contributor III

I got it working, the FSYNC delay need setting to 0x0, not default 0x01. also, i have been make the mpc8315e tdm bus working with si3215/si3050 with zaptel in asterisk-1.4.20. thanks for powerpc's powerful performance! i got all working perfect than other CPU!

 

Best regards,

Li

View solution in original post

0 Kudos
1 Reply
444 Views
uolli
Contributor III

I got it working, the FSYNC delay need setting to 0x0, not default 0x01. also, i have been make the mpc8315e tdm bus working with si3215/si3050 with zaptel in asterisk-1.4.20. thanks for powerpc's powerful performance! i got all working perfect than other CPU!

 

Best regards,

Li

0 Kudos