MPC8313 erdb baord with linux2.6.31.1 can not ping outside

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8313 erdb baord with linux2.6.31.1 can not ping outside

783 Views
jane_gu
Contributor I
Is anyone update Linux kernel in the LinuxBSP from Freescale. which version is workable? I tried the linux2.6.31.1. the network seems have problem. when I enable two interfaces, ping will get exception. if i just enable eth1, it looks ok and I can ping outside.
0 Kudos
1 Reply

300 Views
sudo
Contributor I

I am using 2.6.20 kernel, pretty old but works fine. The latest LTIB BSP is 2.6.23, how do you upgrade to 2.6.31?

If your cpu has silicon rev. 2.0 or 2.1, you may need to check the document "Migration from MPC8313E Revision 1.0 to Revision 2.x". Some software modifications are necessary.

0 Kudos