MPC5744P core checker

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5744P core checker

429 次查看
李丽丽
Contributor I

what's the core checker mechanism of MPC5744P?

0 项奖励
2 回复数

367 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

Checker Core_0s operates in lock step mode with Main Core_0, executing exactly the same instructions as Main Core_0. Thus, Checker Core_0s checks to insure that Main Core_0 is executing correctly. RCCU (Redundancy control checker unit) continuously monitor lock step and if it founds inconsistency it reports this fault to FCCU. In FCCU you can decide whenever you like to trigger interrupt, reset or signal it to outside world. The Checker core and RCCU are disabled in debug mode and it runs in normal mode (no need to enable it manually).

Regards,

Lukas

0 项奖励

367 次查看
李丽丽
Contributor I

OK, thanks.whether there is some details document for core checking

0 项奖励