Hi,
I am working on Interrupt control monitor and there are three IRQs that are monitored. The monitor mode is set to EOI (see the attached picture). In that mode if IRQ latency exceeds that is set in LAT register, error should be signaled, but in the whole reference manual it doesn't says where it will be signaled. Can someone help me with this?
In my case if the IRQ exceeds the latency then INTC_MONITOR0 in FCCU resets my board, even though I set register to no reset reaction.
So if someone can explain me where will the error be signaled I would be very thankful.
已解决! 转到解答。
Yes, I am referring to this
Enabling of any fault reaction enables FOSU counter. You just need to clear the fault before ALARM period expires.
Pay attention to following appnote:
https://www.nxp.com/docs/en/application-note/AN5284.pdf
Yes, I am referring to this
Enabling of any fault reaction enables FOSU counter. You just need to clear the fault before ALARM period expires.
Pay attention to following appnote:
https://www.nxp.com/docs/en/application-note/AN5284.pdf
Hi, it goes over FCCU. If you don't have enabled reset reaction to this fault, but you have enabled another one, it means also FOSU is active and it may reset the device if FCCU interrupt is not handled on time. Have you checked MC_RGM_DES? F_FFRR indicated FOSU reset.
In the past I made example for FOSU fault injection, but on different MCU that does not have RGM module. But FCCU works more or less same way.