MPC5566 writing to Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5566 writing to Flash

1,714 Views
Bloodhound
Contributor I

Hi All,

 

I having some trouble writing to the internal Flash memory, I can erase the flash blocks fine.

I think my problem is I am not really understanding the steps in the MPC manual for programming.

Ignoring the process of unlocking the blocks (which I'm sure I have right), the MPC manual states:

"Write the first address to be programmed in the flash module with the program data."

 

A sampe of my code I am using for testing is to write the data $12345678 to address 0x0006_0000

 

 lis          r12,6           ; Hardcode to address $60000 for testing
 lis          r11,1234
 ori          r11,r11,5678    ; Try to write 12345678 to $60000
 stw          r11,0(r12)

 

Then turn on the EHV bit.

 

But this doesn't work, in fact it makes the CPU reset.

Am I missing something?

 

Thanks.

 

0 Kudos
Reply
2 Replies

727 Views
dayve
NXP Employee
NXP Employee

Hey Bloodhound,

 

We provide flash drivers with an API for writing to the flash on the MPC55xx MCU's. I would recommed that you uses these drivers as the handle the set up of the flash for sucessful programming.

 

Here if the link to the drivers:

MPC55XX_FLASH_DRIVER

 

Regards,

Dayve

0 Kudos
Reply

727 Views
SABK
Contributor I

the driver is good but it does not run on all the versions of mpc5554!!!

how do i find out which version is my mpc???

0 Kudos
Reply