MPC5565 - Censorship Control Word Erased

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5565 - Censorship Control Word Erased

Jump to solution
1,928 Views
J0102
Contributor I
Hi,
I'm working MPC5565 Controller.The Censorship Control word at address FFFDEo got erased accidently.
Now the lauterbach controller is not giving me acess to flash/erase my code.Bus error is generated if we try to write to any area in flash using data.set command.Anyone have an idea how to enable the flash again.


--
Alban Edit: Please always include FSL Part Number in Message Subject line.



Message Edited by Alban on 2007-10-05 10:28 AM
0 Kudos
Reply
1 Solution
1,021 Views
randyd
NXP Employee
NXP Employee
It is very inportant that when the shadow block (where the cesorship control word resides) is erased that it be reprogrammed with llegal censorship values before the device gets reset.

once the censorship control word is erased, if the device is reset, then the flash is never accessible again. there is no way to recover the flash.

View solution in original post

0 Kudos
Reply
1 Reply
1,022 Views
randyd
NXP Employee
NXP Employee
It is very inportant that when the shadow block (where the cesorship control word resides) is erased that it be reprogrammed with llegal censorship values before the device gets reset.

once the censorship control word is erased, if the device is reset, then the flash is never accessible again. there is no way to recover the flash.

0 Kudos
Reply