MIMXRT595-EVK and G1120B0MIPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT595-EVK and G1120B0MIPI

Jump to solution
1,181 Views
RichardHuang88
Contributor I

Dear NXP,

I have MIMXRT595-EVK and G1120B0MIPI on hand.
I import some SDK examples and it seems that MIMXRT595-EVK can work very well.
The problem occurs when MIMXRT595-EVK and G1120B0MIPI are connected.
I tried to run two display examples: fbdev_freertos and sd_jepg.
But they all failed to light up G1120B0MIPI.
The following is the debug message I saw on Tera Term.

fbdev_freertos: "Set frame buffer xxx times." appears repeatedly, but G1120B0MIPI does not display anything.

sd_jepg:
"Card inserted.
No demo jpeg file!
SD card mount error. Demo stopped!"
But there are two jpg files on my SD.

I don't know where the problem is, would you please help me?
Thank you.

0 Kudos
Reply
1 Solution
1,158 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Please refer to readme.txt to learn how to set up the hardware for display examples, the display panel seems to be the TFT Proto 5" CAPACITIVE board.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,162 Views
RichardHuang88
Contributor I

Sorry for the trouble. After I import the watch demo, my G1120B0MIPI can be lighted up. Thanks.

0 Kudos
Reply
1,159 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Please refer to readme.txt to learn how to set up the hardware for display examples, the display panel seems to be the TFT Proto 5" CAPACITIVE board.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply