Currently, we are working on the DEBIX Model C i.MX93 single board, which has a Cortex-M33 processor named MIMX9352AVTXMAB. I want to communicate with the GPIO pins through this processor, so I am using the MCUXpresso IDE. I have also downloaded the SDK through the MCUXpresso SDK Builder. However, when I try to drag that file into MCUXpresso IDE, I receive an error. I have attached a screenshot of that error. Has anyone faced this issue, or does anyone know the solution to this error
Solved! Go to Solution.