Hi all,
I am using FRDM KW-38,
Is there any turtorial doc to guide how to setting debug flash to my chip`,
I already install J-Link but seems can't refer it.
Hello,
Hope you are doing well. Could you please check the: Getting Started with the FRDM-KW38 | NXP Semiconductors?
Also, were you able to flash your FRDM at least one time? If that is the case, what SDK example did you use?
Regards,
Ricardo
Hi @Ricardo_Zamora ,
I am using "frdmkw38_adv_ext_peripheral_freertos" project,
in origianl code after I import build is OK, but debug will happen issue like below picture.
Now I use "GUI FLASH TOOL" to flash my FRDM, but it still have lots of alert window.
Whatever cancel these alert window, It can successfully flash FRDM.