MCIMX6UL-EVKB I2S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6UL-EVKB I2S

Jump to solution
780 Views
ATAineri
Contributor III

I'm creating hifi audio player and now I want to use I2S for working with my own audio codec. How can I do it if on this board there is no available I2S because of wolfson codec use it.

Labels (1)
1 Solution
634 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

This could be possible by using the two codecs in the same SAI,

Please take a look to this:

Set two sound cards to the same SAI (Linux 4.9 iMX6UL)

 

Also, please take into account that some hardware changes may be needed,

but it could cause damage on your board and/or in the codec.

 

I Haven't tried it, but you could use the Arduino Headers for this purpose. Furthermore, if the pads are not being used for any other functionality,

please take a look to the i.MX 6UL RM and the evaluation board schematic

Schematic

i.MX 6UL RM

 

However we cannot guarantee that this will work, and any damage that it may cause to your board/codec will be at your own risk. I apologize for the inconvenience this may cause to you.

 

Best regards,
Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

2 Replies
634 Views
ATAineri
Contributor III

Thank you, I will try it

0 Kudos
635 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

This could be possible by using the two codecs in the same SAI,

Please take a look to this:

Set two sound cards to the same SAI (Linux 4.9 iMX6UL)

 

Also, please take into account that some hardware changes may be needed,

but it could cause damage on your board and/or in the codec.

 

I Haven't tried it, but you could use the Arduino Headers for this purpose. Furthermore, if the pads are not being used for any other functionality,

please take a look to the i.MX 6UL RM and the evaluation board schematic

Schematic

i.MX 6UL RM

 

However we cannot guarantee that this will work, and any damage that it may cause to your board/codec will be at your own risk. I apologize for the inconvenience this may cause to you.

 

Best regards,
Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------