Hi Sir
I am study the MC35XS3400 that the PWM control for Output Now.
According to the Document
https://www.nxp.com.cn/docs/en/data-sheet/MC35XS3400.pdf
I need to send spi command in MPC5744 for MC35XS3400 that it's can control the PWM of output .
Do you have the sample code of MC35XS3400 and provide to me ?
Thank you.
Solved! Go to Solution.
Hi,
The HS0 – HS3 outputs of the MC35XS3400 can be controlled either using GPIO pins through parallel inputs (IN0 – IN3) or SPI.
Currently we do not have a sample code for the MPC5744 and MC35XS3400, unfortunately.
Generally, all available drivers and example codes for analog products can be found at:
Best regards,
Tomas
Hi Tomas
Thank you for your answer.
According to the AN3831.pdf document
https://www.nxp.com.cn/docs/en/application-note/AN3831.pdf
The eXtreme Switch family includes several part numbers, MC35XS3400, MC10XS3435, MC10XS3412, and MC15XS3400 can used the same sample code.
The example shown on this document is being developed using CodeWarrior™ for the 9S12XEP100, 16 bit microcontroller and the driver created for the MC10XS3412.
But I can not find the source code project in Freescale Web Page www.freescale.com.
Can you help me to find the source code and provide for me please ?
Thank you.
Hi Tomas
This is file which I want.
Thank you for your help very much.