MC35XS3400 SPI driver in MPC5744

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC35XS3400 SPI driver in MPC5744

Jump to solution
879 Views
hsieh_jaros
Contributor I

Hi Sir 

I am study the MC35XS3400 that the PWM control for Output Now.

According to the Document

https://www.nxp.com.cn/docs/en/data-sheet/MC35XS3400.pdf

I need to send spi command in MPC5744 for MC35XS3400 that it's can control the PWM of output .

Do you have the sample code of MC35XS3400 and provide to me ?

Thank you.

0 Kudos
1 Solution
864 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

 

Yes, please see attached.

 

Best regards,

Tomas

View solution in original post

0 Kudos
4 Replies
874 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

 

The HS0 – HS3 outputs of the MC35XS3400 can be controlled either using GPIO pins through parallel inputs (IN0 – IN3) or SPI.

Currently we do not have a sample code for the MPC5744 and MC35XS3400, unfortunately.

Generally, all available drivers and example codes for analog products can be found at:

https://www.nxp.com/design/analog-expert-software-and-tools/sdk-analog-expert-drivers:SDK-ANALOG-DRI...

 

Best regards,

Tomas

 

0 Kudos
870 Views
hsieh_jaros
Contributor I

Hi Tomas

Thank you for your answer.

According to the AN3831.pdf document
https://www.nxp.com.cn/docs/en/application-note/AN3831.pdf


The eXtreme Switch family includes several part numbers, MC35XS3400, MC10XS3435, MC10XS3412, and MC15XS3400 can used the same  sample code.

The example shown on this document is being developed using CodeWarrior™ for the 9S12XEP100, 16 bit microcontroller and the driver created for the MC10XS3412.

But I can not find the source code project in Freescale Web Page www.freescale.com.

Can you help me to find the source code and provide for me please ?

Thank you.

0 Kudos
865 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

 

Yes, please see attached.

 

Best regards,

Tomas

0 Kudos
850 Views
hsieh_jaros
Contributor I

Hi Tomas

This is file which I want.

Thank you for your help very much.

 

0 Kudos