MC33772C Not Responding TPL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33772C Not Responding TPL

Jump to solution
549 Views
christoss
Contributor II

Hello,

I'm trying to establish a communication with the MC33772C over TPL. The transmission seems to work. When data is sent the VCOM line of the IC goes to 5V as expected. The echoed frame is able to be read accurately, but after that no data is sent by the MC3377. The BCC library is used.

Below I've screen-captures from the oscilloscope traces. Measurements on the TPL lines was done across the RDTX_IN+ and RDTX_IN-. For isolation between the MC3377 and MC33664 the suggested HM2102NL and HM2103NL transformers are used respectively.

Thanks in advance,

Christos.

 

TEK00000.PNGTEK00002.PNG 

Edit:

It fails in BCC_AssignCid. Instead of receiving 2, 48bit frames (echo and response from the MC3377), it only receives the echoed frame thus returning BCC_STATUS_COM_TIMEOUT.

static bcc_status_t BCC_AssignCid(bcc_drv_config_t* const drvConfig,
    const bcc_cid_t cid)
{
    uint16_t writeVal, readVal;
    bcc_status_t status;

    /* Check if unassigned node replies. This is the first reading after device
     * reset. */
    /* Note: In SPI communication mode, the device responds with all bit filed
     * set to zero except message counter and the correct CRC to the very first
     * MCU <-> MC33771C/772C message. */
    status = BCC_Reg_Read(drvConfig, BCC_CID_UNASSIG, MC33771C_INIT_OFFSET, 1U, &readVal);
    if ((status != BCC_STATUS_SUCCESS) && (status != BCC_STATUS_COM_NULL))
    {
        return status;
    }
// ...
}

 

Tags (3)
0 Kudos
1 Solution
505 Views
christoss
Contributor II

So turns out that for some reason in bcc.h the "BCC_MSG_IDX_*" pre-compiler defines are defined in a weird (different?, wrong?) order. Numbering them in assenting order from top to bottom fixes the issue (on 3rd party MCUs).

 

View solution in original post

0 Kudos
2 Replies
506 Views
christoss
Contributor II

So turns out that for some reason in bcc.h the "BCC_MSG_IDX_*" pre-compiler defines are defined in a weird (different?, wrong?) order. Numbering them in assenting order from top to bottom fixes the issue (on 3rd party MCUs).

 

0 Kudos
513 Views
christoss
Contributor II
In addition to the above I noticed that the TPL wave is sinusoidal (indicating TPL1?). The MC33772C is a TPL2 device, so a square TPL wave. I couldn't figure out how to change that over on the MC33664. Maybe that's the issue?
0 Kudos