MC33772C 4cell configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33772C 4cell configuration

Jump to solution
1,336 Views
robertoschembar
Contributor II

Hi team,

I want use MC33772C for 4 cells configuration (cell 3 and 4 not connected). In the safety manual (par. 8.1.1 or 13.2.2 of the datasheet) seems that LPF could be removed only for CT4 and all Rbal and Rbalc must be present. But in this article for MC33772B seems that also LPF for CT3 is possible to remove.

Moreover I would to remove Rbalc (connected to CB4:3) and Rbal (connected to CB3 and CB4), and all these pin short to CB2, so Rbal for CB2, terminated these pin too.

If this is not possible, is it necessary that Rbal should be the same as the used cells or could be the same value, but with less power?

thanks

0 Kudos
Reply
1 Solution
1,294 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Roberto,

Yes, please look at Fig. 3 of the same application note: it is aimed at MC33772B, but can be used for the MC33772C as well.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
3 Replies
1,326 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Roberto,

I would recommend you to take a closer look at our AN12536 which explains how to arrange LPF for MC33771/MC33772 when using less than 14/6 cells. 

You can download the AN12536 from this website. 

Capture.JPG

Please make sure you are signed in to nxp.com and select Secure Files. If you do not see the AN12536, please click on "Request additional access" or edit your secure access rights by going to My NXP > Profile. 

In case of any problems with downloading the AN12536, please contact directly our DocStore Support team via support.docstore@nxp.com

Best regards,

Tomas

0 Kudos
Reply
1,321 Views
robertoschembar
Contributor II

Hi Tomas,

Using the Filter type B for MC33771 (fig 2 in AN12536) is OK for Safety with MC33772C?

Best regards,

Roberto

0 Kudos
Reply
1,295 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Roberto,

Yes, please look at Fig. 3 of the same application note: it is aimed at MC33772B, but can be used for the MC33772C as well.

Best regards,

Tomas

0 Kudos
Reply