MC error: Operation timed out (status 0x7)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC error: Operation timed out (status 0x7)

886 Views
gsuresh_12
Contributor II

I am using LS1088ardb_pb board.

While using command ls-addni, I am getting below mentioned error

"MC error: Operation timed out (status 0x7)"

and I am unable to connect the board to the network.

Please suggest, what could be the issue to get this kind of error?

root@localhost:~# ls-addni dpmac.3
MC error: Operation timed out (status 0x7)
root@localhost:~#

 

Regards

Suresh

0 Kudos
3 Replies

864 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please make sure MC firmware and rootfs(restool) are from the same version LSDK.

I assume that your use the latest LSDK 21.08.

1. Download the prebuilt composite firmware image:
$ wget https://www.nxp.com/lgfiles/sdk/lsdk2108/firmware_ls1088ardb_pb_qspiboot.img

2. Program image to QSPI NOR flash 1.

=> sf probe 0:1
=> tftp 0xa0000000 firmware_ls1088ardb_pb_qspiboot.img
=> sf erase 0x0 +$filesize && sf write 0xa0000000 0x0 $filesize

3. Reset and boot the board from QSPI NOR flash 1.

=> qixis_reset

 

You also run the following command in LSDK build environment

$ flex-builder -c mc_bin -a arm64

Get mc firmware image in components/firmware/mc_bin/ls1088a/mc_ls1088a_10.28.1.itb.

Please deploy mc firmware image at 0x00A00000 on QSPI flash.

0 Kudos

861 Views
gsuresh_12
Contributor II

Thank you for your response,

I am unable to do tftp at boot time from qspi 1 because no dpmac.x is working.

Is there any method I can program  mc_ls1088a_10.28.1.itb file on chip directly without using tftp method.

Please suggest how can I load mc_ls1088a_10.28.1.itb into the chip by using CodeWarrior Tap through JTAG?

Regards

Suresh

0 Kudos

856 Views
yipingwang
NXP TechSupport
NXP TechSupport

After install the latest CodeWarrior 10.5.5, please refer to "7.7 Using flash programmer from eclipse IDE" in C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual.pdf to do flash programming in CodeWarrior IDE.

You also could use SD card, I assume that you copy mc_ls1088a_10.28.1.itb to the second partition of SD card, then plug-in SD card to the target board.

$ load mmc 0:2 0xa0000000 mc_ls1088a_10.28.1.itb

0 Kudos