Low power consumptions i.mx8 series processor for Medical applications design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Low power consumptions i.mx8 series processor for Medical applications design

90 Views
anusha57
Contributor I

Hi ,

 

We are looking for low power consumption i.MX8 series processor for your custom design.

below is the power requirements.

  • Input High Voltage: 17V
  • Input Low Voltage: 10V
  • Nominal Voltage: 12V or 16V
  • Max Power draw: 500mA @ 12V or 6W (Target)
  • Low Power Mode: ≤5mA @ 12V or 60mW (Target)

Please suggest suitable processor and share the power consumptions details.

0 Kudos
1 Reply

69 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @anusha57!

Thank you for contacting NXP Support!

 

You can check the power consumption of the next processors in their Application notes.

 

The next processors are designed with different features, please check the features of each one by following the link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

iMX8MN UL

https://www.nxp.com/docs/en/application-note/AN13367.pdf

 

iMX8MN

https://www.nxp.com/docs/en/application-note/AN12778.pdf

 

iMX8ULP

https://www.nxp.com/docs/en/application-note/AN13914.pdf

 

Best Regards!

Chavira

0 Kudos