Looking for NXP Evalution board with espi support with master.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for NXP Evalution board with espi support with master.

754 Views
gauravsuryavans
Contributor II

Hi Community,

I am looking for evalution board with have pin out for espi as master, is there any board from NXP.

Any help would be appreciated.

Regards,

Pankaj

Tags (1)
2 Replies

662 Views
Pavel
NXP Employee
NXP Employee

For example see the following boards:

P5040RDB, P1022DS, P1023RDB, P1024RDB, P1025RDB, TWR-P1025

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

662 Views
gauravsuryavans
Contributor II

Hi PavelChubakov‌,

Thanks for answering.

Regards,

Pankaj

0 Kudos
Reply