Looking for AFT05MS003N Characterization at 70 MHz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for AFT05MS003N Characterization at 70 MHz

1,038 Views
glapin
Contributor I

I'd like to use the ATF05MS003N in the 72-76 MHz band.

The datasheet reference circuit gives Zsource and Zload values for frequencies from 135-174 and 350-520 MHz.

The S parameter file covers 240-1000 MHz.

A similar question mentioned the AFT05MS003N_PDK file, which no longer exists.

How can I get the input and output impedance values for my frequency range (72-76 MHz)?

Labels (1)
  • RF

Tags (1)
0 Kudos
Reply
2 Replies

729 Views
OttawaMan
Contributor I

i am also looking for Zsource and Zload values for AFT05MS003N or AFT05MS004N, working at 200Mhz. Please help. Thanks a lot.

0 Kudos
Reply

933 Views
LPP
NXP Employee
NXP Employee

AFT05MS003N is conditionally stable and may require stability enhancement. For your frequency band, applying series 12 Ohm + shunt 27 Ohm resistors at the gate makes amplifier unconditionally stable.

I performed load pull simulation using ADS model of this transistor.

Vdd=7.5V, Idq=80mA
 Zload = 12.54 + j6.24
 Zinput = 14.32 - j9.1

Input impedance as measured from input series resistor to ground.

Amplifier schematics and performance at 74MHz are attached.

Have a great day,

Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply