LS1046QA PCIe compliance test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046QA PCIe compliance test

259件の閲覧回数
Wennnn
Contributor I

Hi,

     We want to do PCIe compliance test,but currently, we can only run at Gen1 2.5G, the following are the step we perform in the Linux command, Can you help to confirm whether it is correct?

root@ls1046ardb:~# devmem2 0x036000A0
0x036000A0 w 0x0/dev/mem opened.
Memory mapped at address 0xffffb99c2000.
Read at address 0x036000A0 (0xffffb99c20a0): 0x00010003
0010013 2root@ls1046ardb:~# devmem2 0x036000A0 w 0x00010013 2
/dev/mem opened.
Memory mapped at address 0xffff8fb2b000.
Read at address 0x036000A0 (0xffff8fb2b0a0): 0x00010003
Write at address 0x036000A0 (0xffff8fb2b0a0): 0x00010013, readback 0x00010013

1.set link speed to 0011'b ->8G.

2.enter compliance setting .

0 件の賞賛
0 返答(返信)