[LS1028a] Unable to enable RS232 as default serial console from software

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[LS1028a] Unable to enable RS232 as default serial console from software

769 Views
Arathi
Contributor II

Hi NXP Support Team,

We are using LS1028a NXP based processor.
We have both RS232 and RS422 as serial ports. Currently for debugging we are using RS422 as our default serial console[debugging port].

Arathi_0-1672981473636.png

 


We Need to make RS232 as our default serial console(debug port).

We tried changing the RCW register of serial port from RS422 to RS232 but no difference observed.
Both ports are working Independently.

Please help us to enable RS232 as default serial console.

 

Regards,
Arathi

0 Kudos
5 Replies

753 Views
yipingwang
NXP TechSupport
NXP TechSupport

LS1028ARDB integrates 2x DB9 RS232 serial ports, you could try to use atf image for LS1028ARDB provided in LSDK 21.08.

Please download LSDK 21.08 from https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/layerscap...

1. cd flexbuild_lsdk2108

$ source setup.env

$ flex-builder -c rcw -m ls1028ardb

2. Please modify components/firmware/rcw/ls1028ardb/R_SQPP_0x85bb/rcw_1500_gpu600.rcw according to your custom board.

3. $ flex-builder -c rcw -m ls1028ardb

 $ flex-builder -c atf -m ls1028ardb -b xspi

Please deploy build/firmware/atf/ls1028ardb/bl2_flexspi_nor.pbl at "0" of XSPI flash and check whether there is output from RS232 serial.

 

0 Kudos

741 Views
Arathi
Contributor II

Hi @yipingwang,

Compiled the Flexbuild 2108 rcw as per the steps provided and deployed build/firmware/atf/ls1028ardb/bl2_flexspi_nor.pbl at '0' of flash. The output is still displaying on the RS422 (port 0) and no output on RS232 (port 1).

Thanks

Arathi

0 Kudos

729 Views
yipingwang
NXP TechSupport
NXP TechSupport

In atf source code folder flexbuild_lsdk2108/components/firmware/atf, in file plat/nxp/soc-ls1028a/include/soc.h UART address is configured as the following.

/* CCSR space memory Map */
#undef NXP_UART_ADDR
#define NXP_UART_ADDR 0x021C0500

#undef NXP_UART1_ADDR
#define NXP_UART1_ADDR 0x021C0600

In file plat/nxp/soc-ls1028a/ls1028ardb/plat_def.h

/* UART related definition */
#define NXP_CONSOLE_ADDR NXP_UART_ADDR
#define NXP_CONSOLE_BAUDRATE 115200

Please modify the above to the following

#define NXP_CONSOLE_ADDR NXP_UART1_ADDR

Then rebuild atf image with the following command.

$ flex-builder -c atf -m ls1028ardb -b xspi

 

 

0 Kudos

704 Views
Arathi
Contributor II

Hi @yipingwang,

In file flexbuild_lsdk2108/components/firmware/atf/plat/nxp/soc-ls1028a/ls1028ardb/plat_def.h,
modified the macro NXP_CONSOLE_ADDR from NXP_UART_ADDR to NXP_UART1_ADDR and rebuild the atf image using the command

$ flex-builder -c atf -m ls1028ardb -b xspi

We are able to get prints in both RS232 and RS422 consoles but RS232 console in getting hang after loading .pbl and further u-boot prints are not getting loaded.

Can you please let me know if i have to change anything in u-boot source file or in other files to resolve this error.

Thanks,
Arathi

0 Kudos

698 Views
yipingwang
NXP TechSupport
NXP TechSupport

LSDK 21.08 source code is only used for NXP demo board, DDR initialization provided in atf source code for ls1028ardb is not suitable your target board. You need to modify flexbuild_lsdk2108/components/firmware/atf/plat/nxp/soc-ls1028a/ls1028ardb/ddr_init.c according to your custom board.

You could refer to section "5.2.1.1 TF-A DDR Driver" in LSDK 21.08 user manual.

0 Kudos