I cannot find any descriptions about the version std802.1CB in LS1028 ARM datasheet.
by testing redundant, I found that the R-tag only has 4 Bytes in LS1028, but in std802.1CB-2017, the R-tag has 6 Bytes.
it seems that LS1028 board cannot support the std802.1CB-2017version?
Your understanding is correct.
The LS1028A switch was implemented against a pre-standard version 802.1CB-d2-2 (draft 2-2).
RED_TAG is a key area that changed when the spec was ratified.
thanks for your reply.
so can I implement the 802.1 CB-2017 by upgrading firmware?
still, I do not know which version does LS1028A support for TSN serials like Qci, Qbv, Qbu, As, can you conform these versions for me? I can not find any version messages in data sheet. thanks
> can I implement the 802.1 CB-2017 by upgrading firmware?
This is not possible because 4-byte RED_TAG is a hardware limitation.
> which version does LS1028A support for TSN serials like Qci, Qbv, Qbu
IEEE802.1Qci/D2.1
IEEE802.1Qbv/D3.1
IEEE 802.1Qbu/D3.0
Refer to the QorIQ LS1028A Reference Manual, 16.4 TSN-Capable Ethernet Switch.
Thank you so much.
is there any other NXP platforms which can support publish version (not draft version) of TSN serials? such as 802.1CB-2017 and 802.1QBV-2015
> is there any other NXP platforms which can support publish version (not draft version) of TSN serials?
Currently - no.