Hello!
I am using LS1021ATSN board.
And I did a yocto-build for installing the systemd package in it.
The build successfully finished, but after I flashed the built image on a SD card and tried to boot on the board, it halts in a certain log and never progresses.
Below is the log screen where the boot halts
Can you tell me how to fix the issue, please?
Thank you, all in advance!
[ 0.568394] Key type dns_resolver registered
[ 0.568502] ThumbEE CPU extension supported.
[ 0.568517] Registering SWP/SWPB emulation handler
[ 0.569431] printk: console [ttyS0]: printing thread started
[ 0.569490] Loading compiled-in X.509 certificates
[ 0.609988] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit
[ 0.649713] mmc0: new high speed SDHC card at address aaaa
[ 0.663749] mmcblk0: mmc0:aaaa SC16G 14.8 GiB
[ 0.676617] mmcblk0: p1 p2
[ 0.776890] ata1: SATA link down (SStatus 0 SControl 300)
[ 0.828849] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[ 0.981451] EXT4-fs (mmcblk0p2): recovery complete
[ 0.982299] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null). Quota mode: disabled.
[ 0.982386] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 0.983199] devtmpfs: mounted
[ 0.986604] Freeing unused kernel image (initmem) memory: 2048K
[ 0.986916] Run /sbin/init as init process
[ 1.103801] hub 1-1:1.0: USB hub found
[ 1.109185] hub 1-1:1.0: 3 ports detected
[ 1.198939] usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd
[ 1.317561] hub 2-1:1.0: USB hub found
[ 1.321984] hub 2-1:1.0: 3 ports detected