LPC8N04

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC8N04

2,504件の閲覧回数
kang1
Contributor I

LPC8N04.jpg

I want to ask what is the use of the plates in the development board wreath in the figure,Debugging programs and downloading programs seem to have nothing to do with it.

0 件の賞賛
返信
7 返答(返信)

2,499件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, DuKang,

The circuit in the red circle is downloading/debugging circuit, as you know that LPC8N04 has two pins PIO0_10/PIO0_11 as SWD port, with pin 2&4 closed for P7 and P8 jumper, the SWD signals of LPC8N04 is connected to the debugging chip LPC11U35, so you can download/debug the LPC8N04 with usb port of chip LPC11U35.

Hope it can help you

BR

XiangJun Rong

 

 

xiangjun_rong_0-1667358835750.png

 

xiangjun_rong_1-1667359050828.png

 

0 件の賞賛
返信

2,495件の閲覧回数
kang1
Contributor I

Hi,XiangJun Rong:

          Thank you very much for your answer. I also want to ask how to configure the debugging mode of MCUXpresso to download and debug programs through the USB of the development board.

0 件の賞賛
返信

2,492件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

After you input the USB cable, the PC can identify  the USB port, in the device manager of PC, the NXP LPC11Uxx is found as the following pic.

If you use MCUXpresso tools and click "debug", the LPC11Uxx is fou8nd automatically.

 

BR

XiangJun Rong

 

 

xiangjun_rong_0-1667373001567.png

 

0 件の賞賛
返信

2,489件の閲覧回数
kang1
Contributor I

20221103_1.jpg

I point after debugging. Always wait for background operation???

20221103_2.jpg

0 件の賞賛
返信

2,487件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

pls check if the jumper are configured correctly, pin 2&4 must be closed  for P7 and P8 jumper.

BR

XiangJun Rong

 

0 件の賞賛
返信

2,481件の閲覧回数
kang1
Contributor I

The jumper has been changed, but the software interface has been stuck here.

20221104_3.jpg20221104_4.jpg

0 件の賞賛
返信

2,479件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

请拨动一下S1开关,以使LPC8N04被供电。

BR

XiangJun Rong

0 件の賞賛
返信