LNA-MML09212H.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LNA-MML09212H.

568 Views
msalehi
Contributor I

I am planing to make an evaluation board for MML09212H.

could you please help me find gerber file or a layout to start working on?

The input and output return loss is very critical for me, I just wondering for frequency 400MHz and 900Mhz how may  I get a better Return loss? which matching circuits would help me to get improvement of at least 3dB on the return loss?

0 Kudos
Reply
1 Reply

508 Views
LPP
NXP Employee
NXP Employee

Please, S-parameters and DXF layout files of the designs are provided on the product summary page:

https://www.nxp.com/products/rf/rf-amplifiers-low-medium-power/low-noise-amplifiers-lnas/lnas-for-in...

Reference designs from the datasheet provides good enough matching. Actually, it is possible to improve narrowband matching in expense of the bandwidth.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply