LLDP source recipies multiple people build option.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLDP source recipies multiple people build option.

196 Views
ranga_yn
Contributor III

Hello NXP,

we are using LLDP source to add recipes to build the source for NXP .Is that possible multiple user can build parallel with the same source - parallel ,if yes let us know how this can be achieved.

Ex: same source LLDP source 2~3 person building parallel.

Any guide or documents steps will help thank

 

regards,

ranga

Tags (1)
0 Kudos
Reply
3 Replies

73 Views
ranga_yn
Contributor III

Hello NXP,

Thanks for the input,

The requirment is X and Y user has to build same source parallel both have logged in as labadmin to YOCTO source. How to enable both so that they can build same time.

or generic way to make multiple people to build on the same source 

 

regards,

ranga

Tags (1)
0 Kudos
Reply

50 Views
Oswalag
NXP TechSupport
NXP TechSupport

In theory you shouldn't have issues but it doesn't seems to be a good practice, is better if all users have their own user to build.

I don't have an example of the mentioned environment, if after testing your environment you have issues please share a detailed explanation of it to review it. 

 

 

0 Kudos
Reply

94 Views
Oswalag
NXP TechSupport
NXP TechSupport

Yes it is possible by default, (no modifications needed), you can limit the number of parallel connections as explained in chapter 5.5.2 Limiting the Number of Parallel Connections in the yocto dev-manual

https://docs.yoctoproject.org/4.3.3/dev-manual/building.html

BR. 

0 Kudos
Reply