LDMOS PA in class D or E possible ???

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LDMOS PA in class D or E possible ???

646 Views
johnjackson
Contributor I

Forum, I am looking into designing a class D or E high efficiency amplifier operating at 80MHz for a laser ignition system.  I have designed a lot of amplifiers with LDMOS but all were class AB.  I don't see anything online about using LDMOS in these switch mode architectures.  Am I missing something or is there some issue or problem with using LDMOS in these conditions.

Thanks,

John Jackson

rfrus1@gmail.com

Labels (1)
  • RF

0 Kudos
Reply
1 Reply

434 Views
milanbaca
Contributor III

Yes it is possible to use LDMOS PA in class D or E.

0 Kudos
Reply