Hello,
I connected JTAG to custom board which has imx8m plus SOM. For SD card boot, i am using boot mode as 1100 (BOOT_MODE [0:3] ) and SD card is working fine. What boot mode should i use for JTAG to work?
Thank you,
Kartheek
Hi @kartheek!
Thank you for contacting NXP Support!
The board should stay on Uboot or Linux booted.
You can Refer to the AN14120 or the next community post:
https://www.nxp.com.cn/docs/en/application-note/AN14120.pdf
Best Regards!
Chavira