JN5189 wakeup time from sleep

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5189 wakeup time from sleep

980 Views
talhamir49
Contributor III

Hello 

I'm using the JN-5189 DK with the example JN-AN-1246, everything is working good but I'm facing a problem that when my device wakes up from sleep it took 60ms to wake up and consume 3 to 4 mA current.

cd1d9f20-ee34-4563-b197-58bda49f2d74.jpg

 

Attached is the photo of the oscilloscope showing the sensor time taken after wakeup and current consumption.

I'm at the end of the project and I need to minimize the size of the pulse so it can drain the minimum current.

kindly help me out.

 

Thank You 

Regards Talha

0 Kudos
2 Replies

966 Views
talhamir49
Contributor III

Hi,

When the MCU wakes up none of the peripherals are reactive as before going to sleep I turn off all the peripherals. No other device is connected.

0 Kudos

969 Views
nxf56274
NXP Employee
NXP Employee

Hi,

When the mcu wakes up, what peripheral are working? Do you close the console print? Do you insert any other device into the arduino connector?

0 Kudos