Hello
I'm using the JN-5189 DK with the example JN-AN-1246, everything is working good but I'm facing a problem that when my device wakes up from sleep it took 60ms to wake up and consume 3 to 4 mA current.
Attached is the photo of the oscilloscope showing the sensor time taken after wakeup and current consumption.
I'm at the end of the project and I need to minimize the size of the pulse so it can drain the minimum current.
kindly help me out.
Thank You
Regards Talha
Hi,
When the MCU wakes up none of the peripherals are reactive as before going to sleep I turn off all the peripherals. No other device is connected.
Hi,
When the mcu wakes up, what peripheral are working? Do you close the console print? Do you insert any other device into the arduino connector?