Hi, Teams,
We are using DMA_Init(EXAMPLE_DMA) in JN-AN-1243-Zigbee-3-0-Base-Device。
my question:
it indicates address 0x4016060 of EndDevice/Build/mcux/EndDevice_OM15082/EndDevice_OM15082.axf section `.bss' is not within region `RAM0'.
Thanks.
First,I use the code in pin_mux.c of 1243 as follow:
/*s
* Copyright 2019-2020 NXP
* All rights reserved.
*
* SPDX-License-Identifier: BSD-3-Clause
*/
/***********************************************************************************************************************
* This file was generated by the MCUXpresso Config Tools. Any manual edits made to this file
* will be overwritten if the respective MCUXpresso Config Tools is used to update this file.
**********************************************************************************************************************/
/* clang-format off */
/*
* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
!!GlobalInfo
product: Pins v6.0
processor: JN5189
package_id: JN5189HN
mcu_data: ksdk2_0
processor_version: 0.0.0
pin_labels:
- {pin_num: '3', pin_signal: PIO0_0/USART0_SCK/USART1_TXD/PWM0/SPI1_SCK/PDM0_DATA, label: LED0, identifier: LED0}
* BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS ***********
*/
/* clang-format on */
#include "fsl_common.h"
#include "fsl_iocon.h"
#include "pin_mux.h"
/* FUNCTION ************************************************************************************************************
*
* Function Name : BOARD_InitBootPins
* Description : Calls initialization functions.
*
* END ****************************************************************************************************************/
void BOARD_InitBootPins(void)
{
BOARD_InitPins();
}
/* clang-format off */
/*
* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
BOARD_InitPins:
- options: {callFromInitBoot: 'true', coreID: cm4, enableClock: 'true'}
- pin_list:
- {pin_num: '15', peripheral: SWD, signal: SWCLK, pin_signal: PIO0_12/IR_BLASTER/SWCLK/PWM0/I2C1_SCL/SPI0_MOSI/ANA_COMP_OUT, mode: pullUp, slew0: standard, invert: disabled,
filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '16', peripheral: SWD, signal: SWDIO, pin_signal: PIO0_13/SPI1_SSELN2/SWDIO/PWM2/I2C1_SDA/SPI0_SSELN, mode: pullUp, slew0: standard, invert: disabled,
filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '12', peripheral: USART0, signal: RXD, pin_signal: PIO0_9/SPI0_SSELN/USART0_RXD/CT32B1_CAP1/PWM9/USART1_SCK/ADO/PDM1_CLK, mode: pullUp, slew0: standard,
invert: disabled, filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '11', peripheral: USART0, signal: TXD, pin_signal: PIO0_8/SPI0_MOSI/USART0_TXD/CT32B0_MAT0/PWM8/ANA_COMP_OUT/RFTX/PDM1_DATA, mode: pullUp, slew0: standard,
invert: disabled, filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '19', peripheral: SPIFI, signal: CSN, pin_signal: PIO0_16/SPI1_SSELN0/ISO7816_RST/PWM5/I2C0_SDA/PDM1_CLK/SPIFI_CSN, mode: pullUp, slew0: standard, invert: disabled,
filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '22', peripheral: SPIFI, signal: SPIFI_CLK, pin_signal: PIO0_18/SPI1_MISO/ISO7816_IO/CT32B0_MAT1/PWM7/USART0_TXD/SPIFI_CLK, mode: pullDown, slew0: standard,
invert: disabled, filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '24', peripheral: SPIFI, signal: 'SPIFI_IO, 2', pin_signal: PIO0_20/IR_BLASTER/USART1_TXD/PWM8/RFTX/SPIFI_IO2, mode: pullDown, slew0: standard, invert: disabled,
filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '21', peripheral: SPIFI, signal: 'SPIFI_IO, 3', pin_signal: PIO0_17/SPI1_MOSI/ISO7816_CLK/SWO/PWM6/CLK_OUT/SPIFI_IO3, mode: pullDown, slew0: standard,
invert: disabled, filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '23', peripheral: SPIFI, signal: SPIFI_IO0_or_SPIFI_MOSI, pin_signal: PIO0_19/ADO/USART1_RXD/CLK_IN/PWM4/USART0_RXD/SPIFI_IO0, mode: pullDown, slew0: standard,
invert: disabled, filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '25', peripheral: SPIFI, signal: SPIFI_IO1_or_SPIFI_MISO, pin_signal: PIO0_21/IR_BLASTER/USART1_SCK/PWM9/RFRX/SWO/SPIFI_IO1, mode: pullUp, slew0: standard,
invert: disabled, filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
* BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS ***********
*/
/* clang-format on */
/* FUNCTION ************************************************************************************************************
*
* Function Name : BOARD_InitPins
* Description : Configures pin routing and optionally pin electrical features.
*
* END ****************************************************************************************************************/
/* Function assigned for the Cortex-M4 */
void BOARD_InitPins(void)
{
/* Enables the clock for the I/O controller block. 0: Disable. 1: Enable.: 0x01u */
CLOCK_EnableClock(kCLOCK_Iocon);
const uint32_t port0_pin12_config = (/* Pin is configured as SWCLK */
IOCON_PIO_FUNC2 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN12 (coords: 15) is configured as SWCLK */
IOCON_PinMuxSet(IOCON, 0U, 12U, port0_pin12_config);
const uint32_t port0_pin13_config = (/* Pin is configured as SWDIO */
IOCON_PIO_FUNC2 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN13 (coords: 16) is configured as SWDIO */
IOCON_PinMuxSet(IOCON, 0U, 13U, port0_pin13_config);
const uint32_t port0_pin16_config = (/* Pin is configured as SPIFI_CSN */
IOCON_PIO_FUNC7 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN16 (coords: 19) is configured as SPIFI_CSN */
IOCON_PinMuxSet(IOCON, 0U, 16U, port0_pin16_config);
const uint32_t port0_pin17_config = (/* Pin is configured as SPIFI_IO3 */
IOCON_PIO_FUNC7 |
/* Selects pull-down function */
IOCON_PIO_MODE_PULLDOWN |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN17 (coords: 21) is configured as SPIFI_IO3 */
IOCON_PinMuxSet(IOCON, 0U, 17U, port0_pin17_config);
const uint32_t port0_pin18_config = (/* Pin is configured as SPIFI_CLK */
IOCON_PIO_FUNC7 |
/* Selects pull-down function */
IOCON_PIO_MODE_PULLDOWN |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN18 (coords: 22) is configured as SPIFI_CLK */
IOCON_PinMuxSet(IOCON, 0U, 18U, port0_pin18_config);
const uint32_t port0_pin19_config = (/* Pin is configured as SPIFI_IO0 */
IOCON_PIO_FUNC7 |
/* Selects pull-down function */
IOCON_PIO_MODE_PULLDOWN |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN19 (coords: 23) is configured as SPIFI_IO0 */
IOCON_PinMuxSet(IOCON, 0U, 19U, port0_pin19_config);
const uint32_t port0_pin20_config = (/* Pin is configured as SPIFI_IO2 */
IOCON_PIO_FUNC7 |
/* Selects pull-down function */
IOCON_PIO_MODE_PULLDOWN |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN20 (coords: 24) is configured as SPIFI_IO2 */
IOCON_PinMuxSet(IOCON, 0U, 20U, port0_pin20_config);
const uint32_t port0_pin21_config = (/* Pin is configured as SPIFI_IO1 */
IOCON_PIO_FUNC7 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN21 (coords: 25) is configured as SPIFI_IO1 */
IOCON_PinMuxSet(IOCON, 0U, 21U, port0_pin21_config);
const uint32_t port0_pin8_config = (/* Pin is configured as USART0_TXD */
IOCON_PIO_FUNC2 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN8 (coords: 11) is configured as USART0_TXD */
IOCON_PinMuxSet(IOCON, 0U, 8U, port0_pin8_config);
const uint32_t port0_pin9_config = (/* Pin is configured as USART0_RXD */
IOCON_PIO_FUNC2 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN9 (coords: 12) is configured as USART0_RXD */
IOCON_PinMuxSet(IOCON, 0U, 9U, port0_pin9_config);
}
/***********************************************************************************************************************
* EOF
**********************************************************************************************************************/
second,i create a source flie in EndDevice to realize my DMA,the code are as follow:
#define CLOCK_ABSTRACTION
/* Abstract attaching the clock */
#define EXAMPLE_SPIFI_CLK_SRC (kMAIN_CLK_to_SPIFI)
#define EXAMPLE_SPIFI_ATTACH_MAIN_CLK (CLOCK_AttachClk(EXAMPLE_SPIFI_CLK_SRC))
/* Abstract getting the clock */
#define EXAMPLE_SPIFI_CLK (kCLOCK_Spifi)
#define EXAMPLE_SPIFI_CLOCK_FREQ (CLOCK_GetFreq(EXAMPLE_SPIFI_CLK))
#define EXAMPLE_DMA (DMA0)
#define EXAMPLE_SPIFI_CHANNEL (12)
#define EXAMPLE_SPIFI SPIFI
#define PAGE_SIZE (256)
#define SECTOR_SIZE (4096)
#define EXAMPLE_SPI_BAUDRATE (16000000L)
static spifi_dma_handle_t handle;
static dma_handle_t s_DmaHandle;
typedef enum _command_t
{
// RDID, /* Write Status Register */
// RDSR, /* Read Status Register */
// RDCR, /* Read Configuration Register */
// WREN, /* Write Enable */
// WRDI, /* Write Disable */
// WRSR, /* Write Status Register */
// PP4, /* Quad Page Program */
// QPP, /* Quad Input Page Program */
// QREAD, /* 1I-4O read */
// SE, /* Sector Erase */
//READ, /* Read */
//DREAD, /* 1I-2O read */
// READ2, /* 2I-2O read */
// PP, /* Page Program */
// READ4, /* 4I-4O read */
//BE64K, /* Block Erase */
//BE32K, /* Block Erase */
// CE, /* Chip Erase */
// DP, /* Deep Power Down */
RSTEN, /* Reset Enable*/
RST, /* Reset*/
MAX_CMD
} command_t;
/*******************************************************************************
* Variables
******************************************************************************/
spifi_command_t command[] = {
// [RDID] = {4, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x9F},
//[RDSR] = {1, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x05},
//[RDCR] = {4, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x15},
//[WREN] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x06},
//[WRDI] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x04},
//[WRSR] = {3, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x01},
//[PP4] = {PAGE_SIZE, false, kSPIFI_DataOutput, 0, kSPIFI_CommandOpcodeSerial, kSPIFI_CommandOpcodeAddrThreeBytes,0x38},
//[QPP] = {PAGE_SIZE, false, kSPIFI_DataOutput, 0, kSPIFI_CommandDataQuad, kSPIFI_CommandOpcodeAddrThreeBytes, 0x32},
//[QREAD] = {PAGE_SIZE, false, kSPIFI_DataInput, 1, kSPIFI_CommandDataQuad, kSPIFI_CommandOpcodeAddrThreeBytes, 0x6B},
//[SE] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x20},
//[READ] = {PAGE_SIZE, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x03},
//[DREAD] = {PAGE_SIZE, false, kSPIFI_DataInput, 1, kSPIFI_CommandDataQuad, kSPIFI_CommandOpcodeAddrThreeBytes, 0x3B},
//[READ2] = {PAGE_SIZE, false, kSPIFI_DataInput, 1, kSPIFI_CommandOpcodeSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0xBB},
// [PP] = {PAGE_SIZE, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x02},
// [READ4] = {PAGE_SIZE, false, kSPIFI_DataInput, 3, kSPIFI_CommandOpcodeSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0xEB},
// [BE64K] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0xD8},
//[BE32K] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x52},
//[CE] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x60},
//[DP] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0xB9},
[RSTEN] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x66},
[RST] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x99},
};
static volatile bool finished = false;
PUBLIC void callback(SPIFI_Type *base, spifi_dma_handle_t *handle, status_t status, void *userData)
{
finished = true;
}
PUBLIC void flash()
{ spifi_config_t config = {0};
/* Init the boards */
/* Security code to allow debug access */
SYSCON->CODESECURITYPROT = 0x87654320;
/* attach clock for USART(debug console) */
CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);
/* reset FLEXCOMM for USART */
RESET_PeripheralReset(kFC0_RST_SHIFT_RSTn);
BOARD_BootClockRUN();
BOARD_InitDebugConsole();
BOARD_InitPins();
uint32_t sourceClockFreq;
/* Set SPIFI clock source */
CLOCK_AttachClk(EXAMPLE_SPIFI_CLK_SRC);
sourceClockFreq = CLOCK_GetSpifiClkFreq();
/* Set the clock divider */
uint32_t divisor;
/* Do not set null divisor value */
divisor = sourceClockFreq / EXAMPLE_SPI_BAUDRATE;
CLOCK_SetClkDiv(kCLOCK_DivSpifiClk, divisor ? divisor : 1, false);
PRINTF("SPIFI flash dma example started \r\n");
//开始
DMA_Init(EXAMPLE_DMA);
DMA_EnableChannel(EXAMPLE_DMA, EXAMPLE_SPIFI_CHANNEL);//通道12
DMA_CreateHandle(&s_DmaHandle, EXAMPLE_DMA, EXAMPLE_SPIFI_CHANNEL);//通道12
/* Initialize SPIFI */
SPIFI_GetDefaultConfig(&config);
SPIFI_Init(EXAMPLE_SPIFI, &config);
/* Reset the SPIFI to switch to command mode */
SPIFI_ResetCommand(EXAMPLE_SPIFI);
SPIFI_TransferRxCreateHandleDMA(EXAMPLE_SPIFI, &handle, callback, NULL, &s_DmaHandle);
/* Reset Device*/
SPIFI_SetCommand(EXAMPLE_SPIFI, &command[RSTEN]);//重置使能
SPIFI_SetCommand(EXAMPLE_SPIFI, &command[RST]);//重置SPI
}
#define CLOCK_ABSTRACTION
/* Abstract attaching the clock */
#define EXAMPLE_SPIFI_CLK_SRC (kMAIN_CLK_to_SPIFI)
#define EXAMPLE_SPIFI_ATTACH_MAIN_CLK (CLOCK_AttachClk(EXAMPLE_SPIFI_CLK_SRC))
/* Abstract getting the clock */
#define EXAMPLE_SPIFI_CLK (kCLOCK_Spifi)
#define EXAMPLE_SPIFI_CLOCK_FREQ (CLOCK_GetFreq(EXAMPLE_SPIFI_CLK))
#define EXAMPLE_DMA (DMA0)
#define EXAMPLE_SPIFI_CHANNEL (12)
#define EXAMPLE_SPIFI SPIFI
#define PAGE_SIZE (256)
#define SECTOR_SIZE (4096)
#define EXAMPLE_SPI_BAUDRATE (16000000L)
static spifi_dma_handle_t handle;
static dma_handle_t s_DmaHandle;
typedef enum _command_t
{
// RDID, /* Write Status Register */
// RDSR, /* Read Status Register */
// RDCR, /* Read Configuration Register */
// WREN, /* Write Enable */
// WRDI, /* Write Disable */
// WRSR, /* Write Status Register */
// PP4, /* Quad Page Program */
// QPP, /* Quad Input Page Program */
// QREAD, /* 1I-4O read */
// SE, /* Sector Erase */
//READ, /* Read */
//DREAD, /* 1I-2O read */
// READ2, /* 2I-2O read */
// PP, /* Page Program */
// READ4, /* 4I-4O read */
//BE64K, /* Block Erase */
//BE32K, /* Block Erase */
// CE, /* Chip Erase */
// DP, /* Deep Power Down */
RSTEN, /* Reset Enable*/
RST, /* Reset*/
MAX_CMD
} command_t;
/*******************************************************************************
* Variables
******************************************************************************/
spifi_command_t command[] = {
// [RDID] = {4, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x9F},
//[RDSR] = {1, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x05},
//[RDCR] = {4, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x15},
//[WREN] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x06},
//[WRDI] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x04},
//[WRSR] = {3, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x01},
//[PP4] = {PAGE_SIZE, false, kSPIFI_DataOutput, 0, kSPIFI_CommandOpcodeSerial, kSPIFI_CommandOpcodeAddrThreeBytes,0x38},
//[QPP] = {PAGE_SIZE, false, kSPIFI_DataOutput, 0, kSPIFI_CommandDataQuad, kSPIFI_CommandOpcodeAddrThreeBytes, 0x32},
//[QREAD] = {PAGE_SIZE, false, kSPIFI_DataInput, 1, kSPIFI_CommandDataQuad, kSPIFI_CommandOpcodeAddrThreeBytes, 0x6B},
//[SE] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x20},
//[READ] = {PAGE_SIZE, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x03},
//[DREAD] = {PAGE_SIZE, false, kSPIFI_DataInput, 1, kSPIFI_CommandDataQuad, kSPIFI_CommandOpcodeAddrThreeBytes, 0x3B},
//[READ2] = {PAGE_SIZE, false, kSPIFI_DataInput, 1, kSPIFI_CommandOpcodeSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0xBB},
// [PP] = {PAGE_SIZE, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x02},
// [READ4] = {PAGE_SIZE, false, kSPIFI_DataInput, 3, kSPIFI_CommandOpcodeSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0xEB},
// [BE64K] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0xD8},
//[BE32K] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x52},
//[CE] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x60},
//[DP] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0xB9},
[RSTEN] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x66},
[RST] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x99},
};
static volatile bool finished = false;
PUBLIC void callback(SPIFI_Type *base, spifi_dma_handle_t *handle, status_t status, void *userData)
{
finished = true;
}
PUBLIC void flash()
{ spifi_config_t config = {0};
/* Init the boards */
/* Security code to allow debug access */
SYSCON->CODESECURITYPROT = 0x87654320;
/* attach clock for USART(debug console) */
CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);
/* reset FLEXCOMM for USART */
RESET_PeripheralReset(kFC0_RST_SHIFT_RSTn);
BOARD_BootClockRUN();
BOARD_InitDebugConsole();
BOARD_InitPins();
uint32_t sourceClockFreq;
/* Set SPIFI clock source */
CLOCK_AttachClk(EXAMPLE_SPIFI_CLK_SRC);
sourceClockFreq = CLOCK_GetSpifiClkFreq();
/* Set the clock divider */
uint32_t divisor;
/* Do not set null divisor value */
divisor = sourceClockFreq / EXAMPLE_SPI_BAUDRATE;
CLOCK_SetClkDiv(kCLOCK_DivSpifiClk, divisor ? divisor : 1, false);
PRINTF("SPIFI flash dma example started \r\n");
//开始
DMA_Init(EXAMPLE_DMA);
DMA_EnableChannel(EXAMPLE_DMA, EXAMPLE_SPIFI_CHANNEL);//通道12
DMA_CreateHandle(&s_DmaHandle, EXAMPLE_DMA, EXAMPLE_SPIFI_CHANNEL);//通道12
/* Initialize SPIFI */
SPIFI_GetDefaultConfig(&config);
SPIFI_Init(EXAMPLE_SPIFI, &config);
/* Reset the SPIFI to switch to command mode */
SPIFI_ResetCommand(EXAMPLE_SPIFI);
SPIFI_TransferRxCreateHandleDMA(EXAMPLE_SPIFI, &handle, callback, NULL, &s_DmaHandle);
/* Reset Device*/
SPIFI_SetCommand(EXAMPLE_SPIFI, &command[RSTEN]);//重置使能
SPIFI_SetCommand(EXAMPLE_SPIFI, &command[RST]);//重置SPI
}
My question :When i call the function flash i created ,
it indicates address 0x4016060 of EndDevice/Build/mcux/EndDevice_OM15082/EndDevice_OM15082.axf section `.bss' is not within region `RAM0'.
Thanks.
Hello,
Could you please give us more details about your question? Did you modify the JN-AN-1243? What AN version are you using? (You can find the version on the Version.txt file) What SDK version are you using?
Regards,
Ricardo
Thank you for your reply .I modify the pin_mux.c and pin_mux.h of 1243.The version of AN is 2006.SDK version is 2.6.5(2022-3-10).
Hi,
Thank you, but could you please let us know the modifications you made?
And also, could you clarify your original question?
Regards,
Ricardo