Is it possible to split a single eDP channel into two seperate LVDS outputs with the PTN3460BS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to split a single eDP channel into two seperate LVDS outputs with the PTN3460BS?

ソリューションへジャンプ
970件の閲覧回数
etidemand
Contributor II

Hi all,

I am looking for a simple way to convert the eDP video stream I'm receiving from my host into LVDS for output to my two displays. In my application I receive LVDS display channel 1 and 2 in a single eDP stream, which I split down the middle and output to my displays from there. My current eDP->LVDS conversion solution uses a multitude of chips and I was hoping I'd be able to redesign that whole thing into a single part, namely the PTN3460BS. I have some questions in this regard:

1. Is the PTN3460BS capable of two unique LVDS outputs?

2. Is it possible for me to split an eDP channel as part of the conversion the PTN3460BS is performing for me?

Thanks and please let me know if I can provide any more information to be more clear!

-Erik

0 件の賞賛
1 解決策
792件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Erik,

PTN3460 can support dual LVDS channel, but same display. It cannot split a single eDP channel into two separate LVDS output. That is the function of a Hub. PTN3460 does not have hub function.

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
793件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Erik,

PTN3460 can support dual LVDS channel, but same display. It cannot split a single eDP channel into two separate LVDS output. That is the function of a Hub. PTN3460 does not have hub function.

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.

0 件の賞賛
792件の閲覧回数
etidemand
Contributor II

Hi Tomas,

Thank you for the information, this is just what I was looking for.

-Erik

0 件の賞賛