Interfacing MC33771B with Arduino UNO using SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Interfacing MC33771B with Arduino UNO using SPI

跳至解决方案
7,179 次查看
ashutosh_saxena
Contributor I

I want help with interfacing MC33771B with Arduino UNO using SPI communication. I am trying to receive the cell values of my battery pack, but I am unable to do so. Can anyone help me with example codes or if someone has already worked on the same, can you please share the code.

0 项奖励
回复
1 解答
7,113 次查看
guoweisun
NXP TechSupport
NXP TechSupport

You can refer to below picture showed code, this GUI design based on KL25Z.

guoweisun_0-1668066910266.png

 

在原帖中查看解决方案

0 项奖励
回复
14 回复数
7,158 次查看
guoweisun
NXP TechSupport
NXP TechSupport

You can sign NDA then download it in the NXP website.

Search | NXP Semiconductors

guoweisun_0-1667980727346.png

 

0 项奖励
回复
7,158 次查看
guoweisun
NXP TechSupport
NXP TechSupport
0 项奖励
回复
7,153 次查看
ashutosh_saxena
Contributor I

We have already downloaded BCC driver software and it is not helping us to establish SPI communication/ fetch data.

0 项奖励
回复
7,156 次查看
ashutosh_saxena
Contributor I

Our company has signed NDA with NXP earlier. 

0 项奖励
回复
7,152 次查看
guoweisun
NXP TechSupport
NXP TechSupport

You can try to directly download it!

0 项奖励
回复
7,118 次查看
ashutosh_saxena
Contributor I

It shows Arduino as an option in Eval GUI, but it is not selectable. How can I solve this?

0 项奖励
回复
7,116 次查看
guoweisun
NXP TechSupport
NXP TechSupport

 

guoweisun_0-1668065400366.png

You can try to re-set the jumper in the FRDM33771BSPIEVB.

 

0 项奖励
回复
7,114 次查看
ashutosh_saxena
Contributor I

Tried that multiple times, but it is not acknowledging Arduino even after updating the port in device manager. 

0 项奖励
回复
7,114 次查看
guoweisun
NXP TechSupport
NXP TechSupport

You can refer to below picture showed code, this GUI design based on KL25Z.

guoweisun_0-1668066910266.png

 

0 项奖励
回复
7,112 次查看
guoweisun
NXP TechSupport
NXP TechSupport

What's your control board? KL25Z? S32?

 

0 项奖励
回复
7,110 次查看
ashutosh_saxena
Contributor I

As of now I am using Arduino as control board and MC33771B as AFE (Cell controller).

0 项奖励
回复
7,140 次查看
ashutosh_saxena
Contributor I

The examples given in the BCC driver folder are for NXP MCU and NXP AFE. I want to configure NXP AFE (MC33771B)  with Arduino UNO.

0 项奖励
回复
4,949 次查看
Shobha
Contributor I

Hey I want to interface MC33771(BCC) with Arduino. Could you pl help me with this if you got the solution for your doubts mentioned here.

0 项奖励
回复
7,128 次查看
ashutosh_saxena
Contributor I

If I have S32K144 evaluation board, will I be able to establish SPI successfully? Is it the same programming that is available in S32 DS ARM IDE.

0 项奖励
回复