Hello Team,
I am using a high-speed CAN transceiver, TJA1042T/3.I have two questions about this product.
1. This IC supports ISO 11898 but SAE J1939?
2. Data rate support is Max 5Mbps, but how much MIN rate is supported?
Thank you in advance.
1:The TJA1042 implements the CAN physical layer as defined in ISO 11898-2:2016 andSAE J2284-1 to SAE J2284-5.
2:You can consider about this limits the minimum bit rate to 60 kbit/s.