IMX8M Plus (L5.4.70-2.3.0_images_MX8MPEVK) Flash Successful, but NPU Execution Fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M Plus (L5.4.70-2.3.0_images_MX8MPEVK) Flash Successful, but NPU Execution Fails

Jump to solution
199 Views
PoojaSk
Contributor I

Hi,

Flashed the pre-built image of linux bsp in IMX8M plus Evk board successfully, using the following steps:
sudo uuu L5.4.70-2.3.0_images_MX8MPEVK.zip
The uuu version used is "libuuu_1.5.201-7-g40bd85c". How can I run the demo applications using NPU. The libvx_delegate.so which is used for the same seems missing. Is there any other way to proceed.


Also, I have initially tried flashing the latest Linux BSP versions such as LF_v6.6.52-2.120_images_IMX8MPEVK. But the process got killed while flashing is there any way to solve it as well. 
This is an urgent requirement, so I’d appreciate a quick response.

Thanks

0 Kudos
Reply
1 Solution
178 Views
Chavira
NXP TechSupport
NXP TechSupport

HI @PoojaSk!

 

Try using the version 1.5.182 this version is the latest stable version of the tool.

To flash the board try decompressing the BSP 6.6.52 and try the next command:

 

sudo uuu -b emmc_all imx-boot-imx8mpevk-sd.bin-flash_evk imx-image-full-imx8mpevk.wic

 

Best Regards!

Chavira

View solution in original post

0 Kudos
Reply
2 Replies
88 Views
PoojaSk
Contributor I

Hi @Chavira ,

The solution helped thanks

0 Kudos
Reply
179 Views
Chavira
NXP TechSupport
NXP TechSupport

HI @PoojaSk!

 

Try using the version 1.5.182 this version is the latest stable version of the tool.

To flash the board try decompressing the BSP 6.6.52 and try the next command:

 

sudo uuu -b emmc_all imx-boot-imx8mpevk-sd.bin-flash_evk imx-image-full-imx8mpevk.wic

 

Best Regards!

Chavira

0 Kudos
Reply