Hi,
Flashed the pre-built image of linux bsp in IMX8M plus Evk board successfully, using the following steps:
sudo uuu L5.4.70-2.3.0_images_MX8MPEVK.zip
The uuu version used is "libuuu_1.5.201-7-g40bd85c". How can I run the demo applications using NPU. The libvx_delegate.so which is used for the same seems missing. Is there any other way to proceed.
Also, I have initially tried flashing the latest Linux BSP versions such as LF_v6.6.52-2.120_images_IMX8MPEVK. But the process got killed while flashing is there any way to solve it as well.
This is an urgent requirement, so I’d appreciate a quick response.
Thanks