IMX 8ULP : PWM buzzer showing delayed sound output after giving variable frequencies

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX 8ULP : PWM buzzer showing delayed sound output after giving variable frequencies

772 Views
Namitha_zcs
Contributor I

I am working on the i.MX8ULP platform using Linux BSP version 6.6, built with the Yocto Project. For implementing the buzzer functionality, I used the "fsl,imx7ulp-pwm"driver. However, there is an issue when setting different frequencies-the buzzer sound is generated only after a significant delay (more than 2 minutes). In contrast, when using a fixed frequency and varying only the duty cycle, the buzzer output works as expected.

0 Kudos
Reply
3 Replies

751 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share how are you changing the frequency?
Is it directly using the device tree?

Best regards/Saludos,
Aldo.

0 Kudos
Reply

696 Views
Namitha_zcs
Contributor I

Hi AldoG ,
I am changing the frequency dynamically from the user space. I am attaching sreenshot for your reference.

Best Regards,
Namitha K Nair

0 Kudos
Reply

532 Views
Namitha_zcs
Contributor I
I wanted to follow up on the issue I raised earlier. As I’m currently working under a tight schedule, I would greatly appreciate any updates or guidance to the solution.
0 Kudos
Reply