IMX 8ULP : PWM buzzer showing delayed sound output after giving variable frequencies

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX 8ULP : PWM buzzer showing delayed sound output after giving variable frequencies

770件の閲覧回数
Namitha_zcs
Contributor I

I am working on the i.MX8ULP platform using Linux BSP version 6.6, built with the Yocto Project. For implementing the buzzer functionality, I used the "fsl,imx7ulp-pwm"driver. However, there is an issue when setting different frequencies-the buzzer sound is generated only after a significant delay (more than 2 minutes). In contrast, when using a fixed frequency and varying only the duty cycle, the buzzer output works as expected.

0 件の賞賛
返信
3 返答(返信)

749件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share how are you changing the frequency?
Is it directly using the device tree?

Best regards/Saludos,
Aldo.

0 件の賞賛
返信

694件の閲覧回数
Namitha_zcs
Contributor I

Hi AldoG ,
I am changing the frequency dynamically from the user space. I am attaching sreenshot for your reference.

Best Regards,
Namitha K Nair

0 件の賞賛
返信

530件の閲覧回数
Namitha_zcs
Contributor I
I wanted to follow up on the issue I raised earlier. As I’m currently working under a tight schedule, I would greatly appreciate any updates or guidance to the solution.
0 件の賞賛
返信